AnsweredAssumed Answered

Verify MMEM:STOR created file correctly via USB

Question asked by evan_davis on Mar 1, 2017
Latest reply on Jan 14, 2021 by Suman1101

I am connecting to an N9020B via the USB interface and running a Python script that does screen captures to a USB drive using the MMEM:STOR:SCR <filename> command. As far as I can tell, there is no way to copy the screen captures back to the PC via USB interface but I would like to verify that the file was created correctly. For instance, if the user forgot to plug a USB drive in, I would like my python script to alert them that the MMEM:STOR:SCR command failed because the drive is not there. Is that possible?

Outcomes