AnsweredAssumed Answered

Lumped element in ADS momentum

Question asked by Mansour001 on Feb 22, 2017
Latest reply on Mar 14, 2017 by bafisher

Hello Everybody,

I would like to make a co-simulation between ADS momentum and layout,

first, i created the metalization path layout in ADS momentum, then i added all ports within the desired place i want to attach the lumped elements.

The question is, the port type of lumped element should be either a port or a pin layout, however for the latter case the schematic simulation hasn't any results

For the port type case, there is an error due to the pin-count numbers in em-model and the concerning symbol representing it, also for this type i assign the +vd and -ve terminal (according to the flowing of current direction), so that means combines 2 pins in one port (Is the problem due to such process??)

If so, how can i assign the current flowing without affecting the number of pins



Outcomes