AnsweredAssumed Answered

Enable source ALC hardware circuit with DCOM

Question asked by andeezlemoyo on Feb 17, 2017
Latest reply on Feb 21, 2017 by daras

Hello, I'm using N5247A with A.10.49.10, and DCOM.

On the "Receiver Leveling Setup" dialog, under the frame, "Controlled Source Setup," the option check box, "Enable Source ALC hardware circuit," how can I set it with DCOM?

I have pulse mod on src1 with 4 pulse generators, and I am using standard pulse profile.

I am fully calibrated including source calibration.

I want to use receiver leveling with the ALC hardware circuit while pulsing, which the docs say is ok.  But I can't find a way to set that setting through DCOM.  So help is needed, thank you.

Andy

Attachments

Outcomes