Hello,
I want to do a FM modulation at 150Hz with 50Hz deviation while the carrier signal goes from 5Khz to 100Hz in 30 second.
Currently I'm using an Agilent 33522a and can do FM modulation or the sweeping separately and as mentioned in the Manual at any given time only one type of modulation is allowed.
My question is, Is there a way to create such a signal? Can I use another waveform generator and try to mix two signals? Is there an easier way to achieve this by building an analog circuit?!
I would appreciate any help and recommendation.
Thanks,
Leo