AnsweredAssumed Answered

What's the best/worst application note on offset loss of cal standard?

Question asked by drkirkby on Jan 28, 2017

I believe i read that there's an Agilent application note that has an error in the description of offset loss. Can anyone tell me what that one is, so I don't confuse myself reading erroneous information.

 

I am looking to find something that can tell me the impedance of the standards in a kit like the 85032B, where the short srandards are not exactly 50 Ohms, but around 49.9 Ohms from memory. 

 

Dave

Outcomes