Hi, I'm currently studying how to use EMPro and have a problem using it. I created microstrip patch antenna and want to see the radiation pattern. When I look at the Advanced Visualization window, it shows the radiation pattern is circle (at Theta 90)(in picture 1). On the other hand, When I look at the Results window (with Far-field Sensor), it shows something else(Picture 2 and 3). I would like to ask if I miss understand how to plot radiation pattern in the Results window.
Be sure you are using the same frequency for displaying results both in the advanced visualization window and the results viewer. Also make sure you are cutting the correct plane with your far field sensor. There are a couple great examples in the help menu if you need to see how it has been done by someone more experienced in EMPro.