I need to log data at a rate of a few kHz, and need a time stamp (at least at the start of the collection period). The non-Pro version seems to have a max rate of 2 Hz. (I can save data from a sweep, but it seems to give a time stamp of when the file is generated rather than when the data is collected.)
Use BenchVue 2017. And be sure to check out the new Scope app with many feature enhancements, coming in a couple of months!
Brian