Does anyone know the proper calibration constants for a first generation 83630A generator? Serial prefix is 3009. Or does anyone have a manual that lists them all. Specifically #463 and #464 and all the board revision #'s.
83620A is 144 as the base code. All the option codes are the same.
example 83620A = 144 so unit with 1,4,6,8 = 144 - 128 + 2 + 4096 = 4114
OPT 001 = -128
OPT 006 = +2
OPT 008 = nothing, 0
OPT 004 = +4096
83622A 128 / 83623A 152 / 83624A 136 / 83640A 176 / 83642A 160 /
83620A is 144 as the base code. All the option codes are the same.
example 83620A = 144 so unit with 1,4,6,8 = 144 - 128 + 2 + 4096 = 4114
OPT 001 = -128
OPT 006 = +2
OPT 008 = nothing, 0
OPT 004 = +4096
83622A 128 / 83623A 152 / 83624A 136 / 83640A 176 / 83642A 160 /