AnsweredAssumed Answered

Performing cal kit uncertainty characterization using ECal

Question asked by lathos on Jan 13, 2017
Latest reply on Jan 15, 2017 by lathos

I am looking to perform a characterization of a mechanical SOLT calibration kit using the new dynamic uncertainty option. It says in the help file that you can use an ECal, where my model (67 GHz) is listed as supported, to calibrate the PNA-X prior to the measurements and embed its traceable uncertainty. However, I cannot see the connected ECal as an uncertainty cal. kit in the Cal. Wizard, and cannot see it in the Cal Kit Manager in the uncertainty application. Do I need to add it somehow, or could it be the case that our unit does not have an uncertainty characterization embedded into it? Or is it on a CD somewhere  ?

 

Thanks in advance!

Outcomes