AnsweredAssumed Answered

IGlobalPowerLimit Interface, 2 internal sources

Question asked by andeezlemoyo on Jan 3, 2017
Latest reply on Jan 9, 2017 by daras

I'm using N5247A with A.10.49.10, and DCOM.

Is there a way to programmatically set the global power limits for the second source?

I'm using the IGlobalPowerLimit interface, which takes a port number.  I have no problem with Port 1 and 2, but the Src2 outs, how can I reference Src2Out1, Src2Out2 ?

By observation, it currently looks like the limit is set for the port specified, for each source.

Any help is greatly appreciated.

Thank you,

Andy

Outcomes