AnsweredAssumed Answered

Connecting multiple pulse (voltage) generator to generate multiple pulses

Question asked by zdzw on Dec 21, 2016

Hello,

 

I need to generate multiple pulses with different amplitudes and widths (I have an HP 214B and an HP 8003A pulse generators). I figure I can connect multiple pulse generators in series. I will use the first pulse generator to generate the first pulse, at the same time, it triggers the 2nd pulse generator. The 2nd pulse generator generate the pulse after a delay as well as triggering the third pulse generator, with a delay.

 

Please let me know if this configuration is feasible. If not, could you suggest alternative ways to accomplish this. 

 

Thanks alot in advance. 

Outcomes