Press the "Meas" button, add some measurements to a waveform, and select Statistics. Set the Max Count value to 100. The scope won't stop collecting statistics even when the Max Count value reaches 100. The values for Current, Mean, Min, Max, Std Dev continue to update.
Scope Firmware level =4.08.2016071800
Anybody else notice this?
Yes, it is a rolling average with the 100 most recent samples, updated after every acquisition. You can see it more clearly when doing successive single acquisitions.
Yes, you can acquire to 100 memory segments and get the statistics for just those acquisitions. The max count could be returned to infinity--you still get the statistics for the 100 segmented memory acquisitions.
Best Regards,
Pat