what are specifications of ADC embedded in N5244? i am intrested to know how much bandwidth i can examine with N5244. how smaller the signal i can pic with this?
I am going to use it with your 118 option. in short what maximum i can get from ADC with 118 option.
i could not understand well. if your IF is at 8.33MHz, .4MSamples/sec may not be enough to get complete picture. however, if your IF is at baseband level, then it will be sufficent to retrieve all information. may be i am confusing it with DSP. could you please attached some Fast-CW data perticularly with pulse mode?
I just want to reconstruct sinosidal wave at baseband or IF level. will this be possible with VNA using Fast CW?