Hello,
I'm trying to find a way to connect two N6700 B's with 6 modules(of various types) and chain protect mode across both mainframes. Previously we've used the digiport functionality to inhibit the other mainframe if we get an OVP or OCP fault on any of the modules on the offending mainframe. This is not ideal in some situations due to the fact that the supplies will come back up once the OVP/OCP is cleared and inhibit is removed. Is there a way(via hardware or software) to have all supplies(on both mainframes) turn off or go into Protect if an OCP or OVP is detected?
Thanks,
Konrad Nied