AnsweredAssumed Answered

Adjusting the scale for Channels 1 and 2 SIMULTANEOUSLY

Question asked by aaronsky12 on Feb 9, 2010
Latest reply on Feb 9, 2010 by Dr_joel
Is there a way on the front panel of the Agilent VNA 8722ES to adjust the scale/div, reference position, reference value, etc. of BOTH channels 1 and 2 simultaneously? I want both channels to gave the exact same scale and reference position... It is a little slow to adjust the scale/reference of channel 1 and then afterwords adjust the scale/reference of channel 2 when I want them to be the same anyways. Thanks.  

Outcomes