I am trying to interface my DSO6104L with a PC but neither a USB connection nor a LAN connection appears to work. I already have installed the Agilent connection expert, the IVI shared components and the drivers for DSO6104L on my computer.
While the manual:
says that the oscilloscope should be detected automatically, when connected through a USB cable, when I connect the oscilloscope, windows fails to detect it. I have attached a screenshot as well.
I also have tried to connect the oscilloscope through a LAN connection, but to my surprise, even being on the the same subnet, the oscilloscope does not appear in the connection expert. I also tried manual connection by using oscilloscope's IP address, but that too isn't resolving the problem.
Nothing appears on the connection expert even when the oscilloscope is connected both through a USB cable and as well as through LAN. I have attached an image of this as well.
Please let me know how should I proceed.
from the 6000 series manual:
http://literature.cdn.keysight.com/litweb/pdf/54684-97030.pdf
basically get into the scope's LXI webpage (LAN), and enable USB.
To get to the LXI page, use the hostname, which is printed on the label near the oscilloscope’s power cord connection. You can reset the hostname form the LAN RESET button on the front panel; see page 45 in manual.