AnsweredAssumed Answered

N5772A analog voltage monitor

Question asked by gstanley001 on Oct 31, 2016

When the supply is set to the "off" mode either manually or by GPIB control the analog voltage monitor (pin J1-11) goes to -0.84Vdc misrepresenting the actual output voltage.  Is this a deliberate feature or a design bug??

 

It would be very nice to have a schematic of this unit.  I also have a broken N5767A that would be easier to repair with a schematic.  (It also reports -0.84V and never comes on showing IEEE on the FP.)  Any help in this area would be much appreciated.

 

Thanks,

Gerald

Outcomes