AnsweredAssumed Answered

N9310A Indication of External Reference

Question asked by wreeve on Oct 27, 2016
Latest reply on Sep 19, 2017 by EricBaker

How does one determine that the N9310A sig/gen is actually using the external reference oscillator or that the external reference oscillator is valid? There doesn't seem to be an annunciator for the external reference.

 

As far as I can determine, the only way to know if the unit is using the internal or external reference is to go to the setup menu. Or, am I wrong?

 

Whit

Outcomes