I want to perform modulation analysis using Keysight's power measurement application.
Mentioned below are some of the relevant details:
Frequency of oscillator: 66KHz
Jittering frequency - 4% of Fosc.
Modulation frequency - 100Hz.
I have followed all the instructions as mentioned in the manual. The time scale was set to 10ms/div and the modulation test was cancelled automatically.
What might be the problem?
Thanks,
Venkatesh
We are not sure what you are trying to do or what software you are using. Are you using BenchVue PM App or Power Panel? Or something else? Analysis is not part of BenchVue, but you can do some math operations using Test Flow. Have you tried that?
Brian