AnsweredAssumed Answered

Continuous ERR RMT errors when connected to 3511B

Question asked by KarlRRI on Oct 6, 2016

I keep getting an error when loading an ARB from BenchVue. This occurs whether the connection is LAN or USB. The display of the generator says "error with remote interface" ERR RMT is displayed in the upper right corner of the generator. Eventually the error clears and the ARB is loaded but it takes several minutes whether loading an ARB or just changing its output status. Is this a configuration issue?

Outcomes