AnsweredAssumed Answered

DSO91304A Trigger on Pulsewidth deviation from nominal

Question asked by volkerlahr on Oct 5, 2016
Latest reply on Oct 10, 2016 by pat_white

DSO91304A

I need to trigger on single periods of a 50MHz squarewave signal with pulsewidth deviating from 50% period length.

However, the pulswidth trigger menu offers only one threshold for triggering, so i can only catch pulses that are either too long or too short, but not both of them.

Any suggestions?

Volker

Outcomes