How do I switch the N6762A-2UA to 0.0002A and back to 0.1A mode using C++? Could not find the API function anywhere. AgilentN67xxOutputFourWiresSenseEnum does not have a function for the 2UA options so is there another library that I can download for that?
Hi Ahmad,
You may refer to the Keysight Series N6700 Low-Profile Modular Power System Programmer’s Reference Guide from Page 101 to 108. The necessary commands to measure and fetch current values are stated in the document.
The link to the reference guide is provided as follows:
Keysight Series N6700 Low-Profile Modular Power System Programmer's Reference Guide