AnsweredAssumed Answered

Momentum: Generate farfield from command line

Question asked by rain_physics on Sep 19, 2016
Latest reply on Oct 18, 2016 by bafisher

I am following the help of ADS-2016.01 Running a momentum from command line 

I have generated S-Parameter successfully using the following command as given in the help

adsMomWrapper -O -3D proj proj 

 

 

In order to generate the farfield, I used the following command as given in the help

adsMomWrapper -FF proj proj 

 

When I execute the above command, I get the following error.

--ERROR-----------------------------------------------

File for view plan proj could not be opened

check   : - existence

               - access permission

 

 

Can anyone suggest me which step I am missing?

Outcomes