Dear *,
I want to get the resistance (I - V) characteristic for a ferrite bead from murata.
So what I need is the DC resistance (max 0.2ohm per datasheet) of ferrite bead for specific current ( from 0A to 1A).
I downloaded the s2p file form murata site for BLM15PX471SN1#.
Is this possible in ADS and how it's done?
Best Regards.
S-parameter data is independent of bias, it is measured at only one operating point, so will not be able to generate meaningful results over any broader operating points. Also this specific s-parameter data file does not contain a 0 Hz measurement, the lowest is 1 MHz, so any simulation at such frequencies will require extrapolation and would not be useful.