I have a 33522 generator controlled by teststand 2014 and with IVI driver ag3352x-x64_2.2.4.0. I unable to set the generator output impedance in High impedance (Hiz) using the Fgen IVI step type.
The IVI Fgen specifications define of an impedance value of 0.0 will place the generator in Hiz. Setting impedance = 0.0 ohm for the generator 33522B will set the output impedance = 1.0 ohm.
How I could set the output impedance to Hi-z using ivi driver and teststand?
Thanks