AnsweredAssumed Answered

control B2987A with matlab through USB

Question asked by BenVerdin on Aug 31, 2016
Latest reply on Sep 1, 2016 by BenVerdin

Hello,

 

I'm trying to control a B2987A (electrometer) with the matlab/IVI driver. I installed the last version of the driver and last found firmware for the instrument.

I use the instrument control toolbox with matlab R2014b. When I scan to find Visa devices, the instrument is identified at the right USB adress (USB0::0x0957::...)  and an interface object is created. When i then try to connect to the device, nothing happens... 

 

Any idea what I'am doing wrong? I could not find any example of script to connect to this device with matlab...

 

Best regards,

 

Benoit

Outcomes