Why can't I adjust the resolution in they Layout window of ADS 21015.01? It no longer appears under the Units/Scle tab of the Options --> Preferences dialog. I have my length units set to mils, but there are 4 trailing decimal points. I don't need that resolution and it flags an error when I try to export the Gerber files, which uses inches and 4 decimal points, but Layout is using 7 (mils + 4 decimal points).
Hello Subby, from the main window go to Options-Technology-Technology Set Up- Layout Units from here you have the option of changing the units and resolution. I also attached a screenshot for your reference.