AnsweredAssumed Answered

Keysight IO - Initiating connection to E8364A very slow!

Question asked by massmog on Aug 8, 2016
Latest reply on Sep 9, 2016 by hognala

Hi all!

I am currently implementing a little measurement procedure in MATLAB, so I am using Agilent IO to connect to a PNA E8364A (V.07.50.37). I can connect to the device, but initiating the connecting takes almost a minute. In the Agilent IO Monitor viGetAttribute (2x) and viOpen each require 15s to complete. Pinging the device works perfectly without delay.

My laptop is connected directly to the PNA using a network patch cable, but my laptop has MDI-X capability.

 

Can anyone give a hint why my connection is so slow?

 

Kind regards,

Max

Outcomes