AnsweredAssumed Answered

8753 port extension in ADS?

Question asked by harvijay on Aug 22, 2011
Latest reply on Aug 22, 2011 by Dr_joel
Hi all,
I am using 8753ES Network analyzer to measure S-par of the MMIC transistor(SOT89 package)
I have two co-ax cables soldered to the input and output of the Transistor with proper bias.
I meassured Port extensions and applied to the NA port extension feature.
It shows accurate values on the screens, but when I try to read S-par using Agilent Intuilink software to save S2P file for ADS simulation, it do not save the port extension(corrected) s-par, but insted it saves uncorrected S-par.
What should I do if I want the corrected S-par? How do i add port extension in to ADS to compensate for error?
Sorry if this question is already asked or not.
Regards.  

Outcomes