AnsweredAssumed Answered

Errors in the alignment on an E4446A

Question asked by theamberco on Jul 13, 2016
Latest reply on Aug 15, 2016 by theamberco

I got alignment errors as indicated in the picture. I replaced the internal battery put the right date and I cleaned the 33325-60009 and the 33326-60009 attenuators and sometimes I dont get the 40dB step error. Do I need to replace both of these modules, This equipment have seen heavy use it has the versión A.11.18. What about the measure Comb error?

I did set the internal ref. 10Mhz out  and connected a cable to the ref out and did the aligment procedure align all.

Any help would be appreciated.

Mike.

aligment erros.jpg

Outcomes