I am trying to change the static IP address in a N9918A FieldFox and continually get Error:Invalid IP address on any field I try to change (IP, SM, GW). I can change from DHCP to Static, and the apply changes field, but nothing else. I've tried rebooting multiple times, as well as with and without cable plugged in.
Any help is much appreciated...
This is an issue that appears when there is nothing in the Static DNS field. Put something like 0.0.0.0 in that field and it should work.