Is there a SPI protocol analyzer available for a 16800 series logic analyzer?
I presently have access to two logic analyzers:
16823A
16804A
I have a 50MHz SPI bus to troubleshoot.
The high sample rate and acquisition buffer depth of these logic analyzers would be great if I can find a SPI decoder to add.
PJ
There used to be one available from Advanced Logical Designs (www.ald.com), but it's apparently not there any more. There are standalone products from several companies that might be useful.