Hi,
I connected Keysight power supply E3648A to PC using NI GPIB cable.
Then pressed I/O config button on front panel and selected GPIB.
Then I ran Keysight connection expert, but it is not detecting my power supply.
Also tried with NI max tool, and some scripts which other teams use. Nothing worked for me.
Later I tried using serial port, that too not working.
Do I have to make any additional settings in the power supply to make it remote enabled?
How can I trouble shoot?
Regards
Ashok Kumar
Hi ashok277,
To resolve this, please uninstall Keysight IO Libraries and NI MAX first. Then, follow exactly the instructions in the Application Note about Tips on using Keysight GPIB Solutions in National Instrument’s LabVIEW Environment.
The link to the application note is provided as follows:
Tips on using Keysight GPIB Solutions in National Instrument's LabVIEW Environment
I hope the above helps!