AnsweredAssumed Answered

Port Extensions

Question asked by NovaBiele on Jun 2, 2016
Latest reply on Dec 1, 2016 by drkirkby

I'm attempting to measure the impedance of an embedded antenna in a device enclosure.  Frequency of operation is 2.45GHz and I have calibrated the reference plane as far as I can go.  I have a 12.4mm feed line going into the enclosure that is attached to a cable at the referenceplane and planned on using the port extension feature to take this extra length into account.

 

When performing the auto-extension method, leaving the feed open & then shorting it , I receive values of 168mm/560ps and 171.5mm/572ps. (I'm using an E5071C)

 

However the physical length of both cables i'm using is 12.4mm/413.6ps. (measures with a ruler, edge of SMA connector to end of the feed line).

 

Is anyone able to explain the discrepency or give some insight as to what I am doing incorrectly?  Thanks.

Outcomes