AnsweredAssumed Answered

PNA-X Dc Meter current measurements crashing

Question asked by rok on May 31, 2016
Latest reply on Jun 2, 2016 by rok

Hi,

 

I'm trying to take DC current measurements from a 34401A multimeter for a Pout vs Pin sweep using a PNA-X with firmware A.10.49.04. The problem is that every time I run the measurement, it gets to the end of the measurement and then crashes the application with this error log:

 

Problem signature:

  Problem Event Name: BEX

  Application Name: 835x.exe

  Application Version: 10.49.550.0

  Application Timestamp: 56d74142

  Fault Module Name: MSVCR100.dll

  Fault Module Version: 10.0.40219.1

  Fault Module Timestamp: 4d5f0c22

  Exception Offset: 0008af3e

  Exception Code: c0000417

  Exception Data: 00000000

  OS Version: 6.1.7601.2.1.0.320.65

  Locale ID: 1033

  Additional Information 1: 8719

  Additional Information 2: 8719d04e26dfb431e5720172b18c6b1a

  Additional Information 3: 19bb

  Additional Information 4: 19bbe2065a25cadcffc4b7e539073637

 

 

Read our privacy statement online:

  http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

 

 

I've attached the .csa file, so if someone can verify the issue and propose a solution, that would be greatly appreciated.

 

Thanks,

rok

Outcomes