When I am analyzing SPI the Lister showing always only 1 entry. I would like to have more entries over time. How to do it?
Are there restrictions like do I have to use the DIGITAL Channel or is it also possible with the 4 Main Channels?
When I am analyzing SPI the Lister showing always only 1 entry. I would like to have more entries over time. How to do it?
Are there restrictions like do I have to use the DIGITAL Channel or is it also possible with the 4 Main Channels?
I checked this option. So I was able to see more than one package in the Lister Window, but the frames come very slow in the Intervall of 300ms so it ended up that the frames are analyzed wrongly.
Is there a possibility to Keep my timebase but to save at least only the SPI Frames in the Lister? Or better the aquisition frames?
You can use segmented memory to do this. Set up the timebase to span your packet, set up a SPI trigger, and enable segmented mode in [Acquire]->Segmented. You can acquire up to 1000 segments and the lister will show all events with time tags across all segments.
Here's an app note on the feature:
http://literature.cdn.keysight.com/litweb/pdf/5990-5817EN.pdf?id=1895166
The lister shows only the number of packets displayed in the last acquisition. You might try slowing your timebase setting to get more packets in the displayed acquisition.