I would like to record with EasyExpert and a B1500a parameter analyzer two curve traces. One from a reference device, one from a failed device. They should appear in the same plot and have different colors. Is that possible with EasyExpert? In the best case scenario I would even be able to append more traces with different colors.
So far I was able to append some curves, but they have all the same color and the legend cannot be edited to label the different curves.
Demo image from another parameter analyzerIn the end it should look like this: