AnsweredAssumed Answered

34980A/34932A Rows failing to close.

Question asked by dpeter001 on May 2, 2016

Has anyone else had intermittent problems with a single row on a 34932A failing to respond to code and/or front panel commands?  When it starts to occur it does not report any error but will fail to open or close until power is cycled on the 34980 chassis.  I should clarify, it seems to accept the open or close command, it just fails to physically change the contacts.  I have seen this on at least 3 different 34980/34932 chassis.  I am doing firmware upgrades now to try to solve it, but I do not see anything about it in the firmware history so I don't hold a lot of hope for it solving the problem.

Outcomes