AnsweredAssumed Answered

PNA-X scpi command for changing x-axis for smc+phase channel

Question asked by rok on Jun 10, 2015
Latest reply on Jun 11, 2015 by daras
Hello,

I am using A.10.40.12 version of the firmware on the PNA-X. I am trying to change the x-axis of 1 of the traces of the smc+phase channel to use the 'input' frequency range instead of the 'output' frequency range. I tried the command:

SENS:MIX:XAX INPUT

i.e. SENS5:MIX:XAX INPUT

but nothing seems to happen at all. I checked for a system error, but did not get any. 

As a followup question, since I have multiple traces within the same SMC+PHASE channel, I want some of the traces's x-axis referenced to the 'input' and some of the other traces referenced to the 'output' range. How can that be done via SCPI commands? In the above command, it is referencing the channel number rather than the trace number.

Thanks,
rok

Outcomes