AnsweredAssumed Answered

The SCPI commands related to 'measure' during an electronic calibration

Question asked by eren on Jan 20, 2016
Latest reply on Jan 27, 2016 by daras
Hello,

         While I calibrate N5242A network analyzer with ECal using SCPI commands, I used "SENS:CORR:COLL:ACQ STAN" +(i+1)  command as an instrument command to fulfill the function of 'Mesure' button in network analyzer display in Agilent VEE program. 'i' value is an input and it is correct (i = 0, 1, 2, etc). The message box 'Connect Noise Source to the port 2 measurement plane' is coming after execution of "SENS:CORR:COLL:ACQ STAN" +(i+1)  command. I am connecting noise source to the port 2 of the network analyzer. Then I am pressing 'OK' button in message box. 'Window 2      No Traces Defined' warning is coming to the display of the network analyzer. I could not find the reason of the error. Must I use a command different than "SENS:CORR:COLL:ACQ STAN" +(i+1)  ?  Can you help me about my problem?

          Regards...  

Outcomes