AnsweredAssumed Answered

N5182B Option Uninstall Question

Question asked by rmax on Sep 2, 2015
Hi, I recently added option 431 to an N5182B and sent the unit to another facility for use. The engineer using this generator informed me there is a problem associated with output power that he did not notice before the addition of the option. Basically he is finding the output power to be about 20 dB lower than set. I don't expect this to be a result of the option add-on but the user would like to uninstall the option to verify whether or not it has anything to do with the problem at hand. I have added many key code options to Keysight equipment in the past but never uninstalled one. Can the option be uninstalled, problem verified, and then reinstalled with the supplied key code?  
Thank you, 
Randy lenox  

Outcomes