AnsweredAssumed Answered

Complex impedance using Network Measurement in 4395A

Question asked by hvempral on Aug 27, 2015
Latest reply on Aug 27, 2015 by drkirkby
Hai all,

I have gone through the 4395A manual to try to figure out as to How to measure the impedance of the DUT. I do not have 010 option as well as S-parameter test set. So, I would be using the Network Measurement function. But as per example shown in 10-7 & 10-8, is it really necessary that I need the S-parameter test set up? Is there any other way to do without it? 

Please do help me.  

Outcomes