AnsweredAssumed Answered

PNA-X Phase noise measurement capability?

Question asked by rok on Jan 6, 2016
Latest reply on Feb 16, 2016 by daras
Hi,

I was wondering if there was some specialized measurement class for the PNA-X that can be used to measure phase noise for amplifiers/converters?

Or is the only way to perform it is to use the PNA-X spectrum analyzer measurement class and use the 'Direct Spectrum' technique? 

Now if we have to use the Opt 90 Enhanced spectrum analyzer to measure phase noise, is there some way to get the 'Band/interval Density Marker' feature that you have on a PXA spectrum analyzer. Or even better, have the 'Option 226 phase noise measurement personality' for the PSA or N9068A Phase Noise Measurement Application for the PXA?

Regards,
rok  

Outcomes