AnsweredAssumed Answered

Query for S Parameter order

Question asked by gfreeman on Oct 8, 2015
Latest reply on Oct 15, 2015 by Dr_joel
I am using the SNP command to get the s parameters back from a PNA-X. Is there a way I can either:
a) Set the order these are returned in 
or b) Query the device for the order they will be returned in

I ask because it seems there is some inconsistency between 2 port and 4 port measurements. The former returns s11,s21,s12,s22 and the latter s11,s12,s13,s14;s21...etc. I am loading this data into a database and want to ensure I have the correct parameter associated with the correct field.  

Outcomes