AnsweredAssumed Answered

8757C has the wrong colors!

Question asked by stu@aptecelectronics.com on Oct 13, 2015
Latest reply on Oct 14, 2015 by stu@aptecelectronics.com
I have two 8757C's and the first one (s/n2932A00921) has the proper colors for ch.1 (yellow) and ch2.(blue)
However the other one (s/n 2834A00407) has ch.1 (white) and ch2. (red) It has no sign of any error messages and works fine except the colors are wrong.
So I swapped parts (display, A14) until I determined the A3 (CPU) assembly is the culprit.
I tried swapping all the ROM's on both boards but that did not change anything. 
So the question is:
did some versions come from the factory with different colors or do I have an elusive problem?  

Attachments

Outcomes