AnsweredAssumed Answered

85062B Ecal 1-26.5GHz

Question asked by theamberco on Sep 9, 2015
Latest reply on Sep 20, 2015 by drkirkby
Hi, I have the above Ecal so how do you suppose to connect the smaller module 1-26.5GHz 85062-60006 to the PNA. The Ecal came with two modules one with only the parallel connector and the other with parallel and an USB port that say use with PNA while the parallel say 85097A/85060C the module is the 85093-60007 , do you need special cables to InterConnect both of the  modules and the connect it to the USB port of the VNA? The manual in here does not say.
Thanks

Edited by: theamberco on Sep 9, 2015 11:46 AM  

Attachments

Outcomes