AnsweredAssumed Answered

Variable definition of component model

Question asked by ipa on May 27, 2015
Latest reply on May 27, 2015 by volker_muehlhaus
I have several identical JFET components in a simulation model.  They are each defined from a JFET model.  To change the device used I have to edit each component and select a different model, JFETM1, JFETM2, JFETM3 ...  Is there a quicker way of doing this ?

Can I use one string variable JFET_TYPE in each of the components to define the the Model name, and a Variable definition JFET_TYPE="JFETM1", to define the actual model referenced ?  I have tried this but can't get it to work, is this possible or is there a better a way ?  

Outcomes