AnsweredAssumed Answered

Fatal Error of the PNA firmware

Question asked by andeezlemoyo on Mar 10, 2015
Latest reply on Mar 11, 2015 by daras
Hi,

I am working with an 2-port E8362C, running firmware version, A.09.42.22.

In my instrument state, I have a trace with an equation that is set to: "Tr3 / Tr6.Mem" .

While the equation is enabled, if I delete the trace, the PNA firmware crashes with a fatal error.

I can also trigger the crash by invoking the Preset.

I can trigger the crash either using DCOM or the front panel. 

If I disable the equation, then everything is fine, i.e. no crash.

I can reproduce the issue from a clean Preset, NO DCOM.  The issue is that I'm using "TrN / TrX.Mem" .  The crash only occurs when I reference 2 different traces is the manner shown, at least that I'm aware of anyway.  

Could you please try to reproduce on your end?

Thank you!!

Andy  

Outcomes