AnsweredAssumed Answered

PFL Licence issue with profiler

Question asked by hlodwig on Feb 15, 2016

Hello,

I have an application using the PFL to drive an equipement (8164B with tunnable laser and photometer).
I need to profile this application. For this purpose, I want to use Dr Memory.
But if I run my application with Dr memory, it's impossible to use the equipment because I have this error message :

"The Agilent PFl is not licenced to run on this computer."

So I checked the licencing tool, the licence is well active. And all works fine if I don't use the profiler.

How can I use it ? Is there a particular thing to configure ?

Best regards.

Outcomes