AnsweredAssumed Answered

PNAX SMC+phase S22 does not update when avg is on

Question asked by rfelectek on May 13, 2015
Latest reply on May 15, 2015 by rfelectek
Good Morning,

We have noticed that when averaging is turned on in SMC+phase measurement class that S22 trace is not updated after first sweep. I believe this has been the case for  in several(if not all) firmware releases through current customer release. Is there some way for me to set the PNAX so S22 will update when averaging is on in this channel where I am also measuring S11 and S21(gain/phase/delay). I realize we can do a workaround but would prefer, for a few reasons, to have it work in currently configured .CSA's. I can send CSA if needed but it should be easy to recreate.

Thanks in advance for taking the time to read and respond  

Outcomes